This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368, standard mode, output YCC16 with embedded sync at 480P, fails

This issue looks very much like another post "DM368 output YCC8 at NTSC with bad vertical parameters". But the situation is worse - HDMI transmitter can not lock to DM368 video output running at standard mode, output YCC16 with embedded sync at 480P. We have cross-examined the HDMI transmitter - it has no problem taking YCC16 input with embedded sync at 480P from an ADC. Now the issue comes down to DM368.

480P and 576P are twins: how 576P is programmed, and so is 480P. The only difference is VENC.VMOD, H/V active, and H/V margin. However, 576P behaves fine while 480P does not.

The following is the register dump:
0x01c71e00: 00000501 00006000 00000000 00000000
0x01c71e10: 0000003e 00000006 00000359 0000007a
0x01c71e20: 000002d0 0000020c 00000024 000001e0
0x01c71e30: 00000000 00000000 00000001 00000000
0x01c71e40: 0000ff00 00000000 00000000 00000001
0x01c71e50: 00000000 00000000 00000000 00000000
0x01c71e60: 00000000 00000800 00000001 00000000
0x01c71e70: 00000000 00000000 00000000 00000000
0x01c71e80: 00000000 00000000 00000000 00000000
0x01c71e90: 00000000 00000000 00000000 00000000
0x01c71ea0: 00000000 00000000 00000000 00000000
0x01c71eb0: 00000000 00000000 00000000 00000000
0x01c71ec0: 00000000 00007000 00000000 0000017a
0x01c71ed0: 00000000 00000000 00000000 00000000
0x01c71ee0: 00000100 00000000 00000000 00000000
0x01c71ef0: 00000000 00000000 00000000 00000000
0x01c71f00: 00000400 0000057c 00000159 000002cb
0x01c71f10: 000006ee 00000400 0000057c 00000159
0x01c71f20: 000002cb 000006ee 00000000 00000000
0x01c71f30: 00000001 00000000 00000000 00000000
0x01c71f40: 00000010 00000000 00000000 00000000
0x01c71f50: 00000000 00000000 00000000 00000000
0x01c71f60: 00000000 00000000 00000000 00000000
0x01c71f70: 0000d642 00000000

Same as the post "DM368 output YCC8 at NTSC with bad vertical parameters", this issue also appears to be a sync issue. Please suggest how we can tune DM368. Thanks in advance.