Hi All,
I was working on customized DM385 som with IPNC RDK 3.5 version.
My usecase is like
Camera -> deiId -> dupId -> display
From dupId.numOutQUe is 2. one output i was using to displayLink and another one I was using to encLink.
In my usecase, when I am trying to create the displayLink, I was getting as assertion issue as the below logs
logs
================================================================================
[m3vpss ] 10240: DISPLAY: Create in progress !!!
[m3video] 10226: ENCODE: All CH Create ... DONE !!!
[m3vpss ] DisplayId = 1,DataFormat = 7
[m3vpss ] SC2 displayInstId = 6
[m3vpss ] KOLANCHI : DisplayLink_drvDisplayCreate 1027, displayHndl is null
[m3video] ENCLINK:HEAPID:0 USED:26040
[m3vpss ] 10242: Assertion @ Line: 1029 in links_m3vpss/display/displayLink_drv.c: pObj->displayHndl != NULL : failed !!!
[m3video] 10229: ENCODE: Create ... DONE !!!
[m3video] 10230: IPC_BITS_OUT : Create in progress !!!
[m3video] 10233: IPC_BITS_OUT : Create Done !!!
================================================================================
I have attached the complete log.
can you figure it out my mistake. Any advise will be highly appreciated!
Regards,
Kolanchi.