Hi,
I'm working with a custom board that relies on a DM368 processor and I'm currently trying to add support for a 29F64G08CBAAA Micron NAND chip. According to the datasheet, it has a 8K + 448 bytes page size. I checked and the silicon revision of the processor I'm using is 1.2 and it is supposed to support such page size (even when they mention that at the time of writing of the technical documents, there were no available NAND pieces to test the RBL support for this page size).
My question is, where can I find the ECC layout for a 8K page size so that I can start adding the support in the bootloader and kernel?
Any help is much appreciated.
Thanks
Diego Chaverri