Hi everybody,
I try to use IPNC RDK 4.0 to drive DM368 + TVP5150, but there is no TVP5150 support in this RDK. Only TVP514X.
Could you share some patch for RDK 4.0 to work with TVP5150?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jesse Sam,
I may not be able to share the patches to you, but I can give some hint. No major changes are required derive tvp5150 driver from tvp514x driver and get basic functionality up. Just modify the tvp514x driver by reffering to tvp5150 data sheet. Consider updating device and addressed while doing so.
Hi ravikiran hv,
Thank you for your replay. I also have done the port from tvp514x to tvp5150 based RDK 4.0 including TVP5150 register setting as datasheet, or compiling macro IMGS_TVP5150 definition in RDK4.0, and it has taken me over one month to debug the procedure, no big further step, only blurry images gotten from the TI web av_capture example. It's a little case for you, however it's a complicated case for me. no indication is software or hardware issue. TVP5150 register dump is attached. I2C: 0x00 = 0x00
I2C: 0x01 = 0x15
I2C: 0x02 = 0x00
I2C: 0x03 = 0x9f
I2C: 0x04 = 0xdc
I2C: 0x05 = 0x00
I2C: 0x06 = 0x10
I2C: 0x07 = 0x60
I2C: 0x08 = 0x00
I2C: 0x09 = 0x80
I2C: 0x0a = 0x80
I2C: 0x0b = 0x00
I2C: 0x0c = 0x80
I2C: 0x0d = 0x47
I2C: 0x0e = 0x00
I2C: 0x0f = 0x12
I2C: 0x10 = 0x00
I2C: 0x11 = 0x00
I2C: 0x12 = 0x00
I2C: 0x13 = 0x00
I2C: 0x14 = 0x00
I2C: 0x15 = 0x01
I2C: 0x16 = 0x80
I2C: 0x17 = 0x80
I2C: 0x18 = 0x00
I2C: 0x19 = 0x00
I2C: 0x1a = 0x0c
I2C: 0x1b = 0x14
I2C: 0x1c = 0x00
I2C: 0x1d = 0x00
I2C: 0x1e = 0x00
I2C: 0x1f = 0x00
I2C: 0x20 = 0x00
I2C: 0x21 = 0x00
I2C: 0x22 = 0x00
I2C: 0x23 = 0x00
I2C: 0x24 = 0x00
I2C: 0x25 = 0x00
I2C: 0x26 = 0x00
I2C: 0x27 = 0x00
I2C: 0x28 = 0x00
I2C: 0x29 = 0x00
I2C: 0x2a = 0x00
I2C: 0x2b = 0x00
I2C: 0x2c = 0x35
I2C: 0x2d = 0x25
I2C: 0x2e = 0x0f
I2C: 0x2f = 0x01
I2C: 0x30 = 0x00
I2C: 0x31 = 0x00
I2C: 0x32 = 0x00
I2C: 0x33 = 0x00
I2C: 0x34 = 0xff
I2C: 0x35 = 0x00
I2C: 0x36 = 0x00
I2C: 0x37 = 0x00
I2C: 0x38 = 0x00
I2C: 0x39 = 0x2e
I2C: 0x3a = 0x01
I2C: 0x3b = 0x3a
I2C: 0x3c = 0x00
I2C: 0x3d = 0x00
I2C: 0x3e = 0x00
I2C: 0x3f = 0x00
I2C: 0x40 = 0x00
I2C: 0x41 = 0x00
I2C: 0x42 = 0x00
I2C: 0x43 = 0x00
I2C: 0x44 = 0x00
I2C: 0x45 = 0x00
I2C: 0x46 = 0x00
I2C: 0x47 = 0x00
I2C: 0x48 = 0x00
I2C: 0x49 = 0x00
I2C: 0x4a = 0x00
I2C: 0x4b = 0x00
I2C: 0x4c = 0x00
I2C: 0x4d = 0x00
I2C: 0x4e = 0x00
I2C: 0x4f = 0x00
I2C: 0x50 = 0x00
I2C: 0x51 = 0x00
I2C: 0x52 = 0x00
I2C: 0x53 = 0x00
I2C: 0x54 = 0x00
I2C: 0x55 = 0x00
I2C: 0x56 = 0x00
I2C: 0x57 = 0x00
I2C: 0x58 = 0x00
I2C: 0x59 = 0x00
I2C: 0x5a = 0x02
I2C: 0x5b = 0x03
I2C: 0x5c = 0x03
I2C: 0x5d = 0x03
I2C: 0x5e = 0x03
I2C: 0x5f = 0x03
I2C: 0x60 = 0x03
I2C: 0x61 = 0x03
I2C: 0x62 = 0x01
I2C: 0x63 = 0x01
I2C: 0x64 = 0x01
I2C: 0x65 = 0x01
I2C: 0x66 = 0x01
I2C: 0x67 = 0x01
I2C: 0x68 = 0x01
I2C: 0x69 = 0x01
I2C: 0x6a = 0x01
I2C: 0x6b = 0x01
I2C: 0x6c = 0x01
I2C: 0x6d = 0x01
I2C: 0x6e = 0x01
I2C: 0x6f = 0x01
I2C: 0x70 = 0x01
I2C: 0x71 = 0x01
I2C: 0x72 = 0x01
I2C: 0x73 = 0x01
I2C: 0x74 = 0x01
I2C: 0x75 = 0x01
I2C: 0x76 = 0x01
I2C: 0x77 = 0x01
I2C: 0x78 = 0x01
I2C: 0x79 = 0x01
I2C: 0x7a = 0x01
I2C: 0x7b = 0x01
I2C: 0x7c = 0x01
I2C: 0x7d = 0x01
I2C: 0x7e = 0x01
I2C: 0x7f = 0x01
I2C: 0x80 = 0xa3
I2C: 0x81 = 0x75
I2C: 0x82 = 0x04
I2C: 0x83 = 0x00
I2C: 0x84 = 0x00
I2C: 0x85 = 0x02
I2C: 0x86 = 0x80
I2C: 0x87 = 0x00
I2C: 0x88 = 0x90
I2C: 0x89 = 0x10
I2C: 0x8a = 0x1a
I2C: 0x8b = 0x00
I2C: 0x8c = 0x81
I2C: 0x8d = 0x01
I2C: 0x8e = 0x02
I2C: 0x8f = 0x01
I2C: 0x90 = 0x00
I2C: 0x91 = 0xdf
I2C: 0x92 = 0xf0
I2C: 0x93 = 0x00
I2C: 0x94 = 0x00
I2C: 0x95 = 0x08
I2C: 0x96 = 0x00
I2C: 0x97 = 0x44
I2C: 0x98 = 0x52
I2C: 0x99 = 0x42
I2C: 0x9a = 0x00
I2C: 0x9b = 0x01
I2C: 0x9c = 0x84
I2C: 0x9d = 0x00
I2C: 0x9e = 0x20
I2C: 0x9f = 0x08
I2C: 0xa0 = 0x08
I2C: 0xa1 = 0x00
I2C: 0xa2 = 0x01
I2C: 0xa3 = 0x20
I2C: 0xa4 = 0x12
I2C: 0xa5 = 0x00
I2C: 0xa6 = 0x20
I2C: 0xa7 = 0x01
I2C: 0xa8 = 0x01
I2C: 0xa9 = 0x88
I2C: 0xaa = 0x48
I2C: 0xab = 0xc4
I2C: 0xac = 0x02
I2C: 0xad = 0x84
I2C: 0xae = 0xb4
I2C: 0xaf = 0x8a
I2C: 0xb0 = 0x60
I2C: 0xb1 = 0x61
I2C: 0xb2 = 0x00
I2C: 0xb3 = 0x22
I2C: 0xb4 = 0x00
I2C: 0xb5 = 0x00
I2C: 0xb6 = 0x04
I2C: 0xb7 = 0x00
I2C: 0xb8 = 0x00
I2C: 0xb9 = 0x00
I2C: 0xba = 0x40
I2C: 0xbb = 0x00
I2C: 0xbc = 0x00
I2C: 0xbd = 0x00
I2C: 0xbe = 0x00
I2C: 0xbf = 0x00
I2C: 0xc0 = 0x57
I2C: 0xc1 = 0x00
I2C: 0xc2 = 0x01
I2C: 0xc3 = 0x2e
I2C: 0xc4 = 0xf0
I2C: 0xc5 = 0x00
I2C: 0xc6 = 0xf1
I2C: 0xc7 = 0x00
I2C: 0xc8 = 0x31
I2C: 0xc9 = 0x00
I2C: 0xca = 0x18
I2C: 0xcb = 0x4e
I2C: 0xcc = 0x00
I2C: 0xcd = 0x00
I2C: 0xce = 0x00
I2C: 0xcf = 0x00
I2C: 0xd0 = 0x00
I2C: 0xd1 = 0x80
I2C: 0xd2 = 0x8f
I2C: 0xd3 = 0x8d
I2C: 0xd4 = 0xff
I2C: 0xd5 = 0x67
I2C: 0xd6 = 0xfa
I2C: 0xd7 = 0xfb
I2C: 0xd8 = 0xff
I2C: 0xd9 = 0xdd
I2C: 0xda = 0xff
I2C: 0xdb = 0xef
I2C: 0xdc = 0xff
I2C: 0xdd = 0xff
I2C: 0xde = 0xff
I2C: 0xdf = 0xff
I2C: 0xe0 = 0xff
I2C: 0xe1 = 0xff
I2C: 0xe2 = 0xff
I2C: 0xe3 = 0xff
I2C: 0xe4 = 0xff
I2C: 0xe5 = 0xff
I2C: 0xe6 = 0xff
I2C: 0xe7 = 0xff
I2C: 0xe8 = 0xff
I2C: 0xe9 = 0xff
I2C: 0xea = 0xff
I2C: 0xeb = 0xff
I2C: 0xec = 0xff
I2C: 0xed = 0xff
I2C: 0xee = 0x95
I2C: 0xef = 0x2d
I2C: 0xf0 = 0xaf
I2C: 0xf1 = 0xd8
I2C: 0xf2 = 0xfb
I2C: 0xf3 = 0xaf
I2C: 0xf4 = 0xef
I2C: 0xf5 = 0xff
I2C: 0xf6 = 0xff
I2C: 0xf7 = 0xe2
I2C: 0xf8 = 0xa7
I2C: 0xf9 = 0x42
I2C: 0xfa = 0xdf
I2C: 0xfb = 0xe1
I2C: 0xfc = 0x47
I2C: 0xfd = 0x00
I2C: 0xfe = 0x00
Could you help to check what's wrong?my email: jsamcnt@gmail.com, your patch will be much appreciated.
Thanks!
Ran,
RDK documentation includes an application note which explains how to integrate an external video decoder.
Regards,
Yair
Sorry folks
Since IPNC is licenced, I don know wether I can share the code. I need to check with our office ppl on this regards.
Hi the code for capturing BT656 should be the same for TVP5150/TVP5147.
However, the register values to initialize the chips should be different. You just need to set 3 registers to enable TVP5150 work.
WR_REG,VID_DEC,1,0x7F,0x00 // Restart CPU
WR_REG,VID_DEC,1,0x0F,0x0A // Select GPCL pin definition
WR_REG,VID_DEC,1,0x03,0x6F // GPCL high (not used), YUV output enable
BR,
Eason