Dear Mr/Mrs,
I'm testing IPNC DM368. And there is a problem.
CMOS imager of the Micron was changed with our customized FPGA.
When output of FPGA is very noisy , IPNC hang up.
Following is my test results.
1. VBR & Noisy image input => hang up
2. CBR & Noisy image input => hang up
3. OFF rate control & Noisy image input => run correctly...
Other settings for testing are
- Codec : H.264
- Stream type : single
-Resolution : H264:D1
-Frame rate : 30
-Bit rate : 4000 kbps.
With CE_DEBUG=3, I have attached log file of IPNC.
Until 106 sec , FPGA outputs normal image.
When about 107 sec, it outputs very noisy image.
How can I solve this issue?
Best regards,