Hi ,
I have a pending issue need your guys help, it is about the
multi-serializer in transmit mode<AXR0 to AXR1> and receive mode<AXR2 to AXR3>.
Individually they work correctly, such as AXR0 for transmit and AXR2 for receive or AXR1 for transmit
and AXR3 for receive. But something wrong happens when I use AXR0、AXR1 for transmit and AXR2、AXR3 for receive simultaneously.
My application is based on ALSA lib + DVRRDK_04.00.00.03, When i capture audio data by call snd_pcm_readi ,
It will be blocked on this function, What can be done to solve this issue?
Please someone help me check the driver modification.
static u8 tvp5158_iis_serializer_direction[] = {
TX_MODE, TX_MODE, RX_MODE, RX_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
};
static struct snd_platform_data tvp5158_snd_data = {
.tx_dma_offset = 0x46000000,
.rx_dma_offset = 0x46000000,
.asp_chan_q = EVENTQ_0,
.tdm_slots = 2, /* number of channels */
.op_mode = DAVINCI_MCASP_IIS_MODE,
.num_serializer = ARRAY_SIZE(tvp5158_iis_serializer_direction),
.serial_dir = tvp5158_iis_serializer_direction,
.version = MCASP_VERSION_2,
/*
* Having Max number of channels as mcasp fifo / edma read depth.
* For 4ch this granularity is still 16 which is ok
*/
.txnumevt = 2,
.rxnumevt = 2,
/* McASP21_AHCLKX out to feed CODEC CLK*/
.clk_input_pin = MCASP_AHCLKX_OUT,
};
static struct resource ti81xx_mcasp0_resource[] = {
{
.name = "mcasp0",
.start = TI81XX_ASP0_BASE,
.end = TI81XX_ASP0_BASE + (SZ_1K * 12) - 1,
.flags = IORESOURCE_MEM,
},
/* TX event */
{
.start = TI81XX_DMA_MCASP0_AXEVT,
.end = TI81XX_DMA_MCASP0_AXEVT,
.flags = IORESOURCE_DMA,
},
/* RX event */
{
.start = TI81XX_DMA_MCASP0_AREVT,
.end = TI81XX_DMA_MCASP0_AREVT,
.flags = IORESOURCE_DMA,
},
};
static struct platform_device ti81xx_mcasp_tvp5158_device = {
.name = "davinci-mcasp", /* driver name */
.id = 0,
.dev = {
.platform_data = &tvp5158_snd_data,
},
.num_resources = ARRAY_SIZE(ti81xx_mcasp0_resource),
.resource = ti81xx_mcasp0_resource,
};
Regards,
tfg