Hi,
I am using tvp5158 connected to dm365 processor with Linux MCVIP driver and dvsdk 4.02. I ported MCVIP driver to work with dvsdk 4.02, modified Davinci video driver to correspond changes made in files in lsp_patch director. My application captures videos from tvp5158 inputs, passes them through resizer, compress them using h.264 encoder and send to writer task that save video to files.
I tried the application with 2ch D1, 4 ch CIF and with 4ch D1 and I have a problem when capturing 4ch D1 videos. When there is no movement in video picture is good but during motion it seems that moving parts of video are not continuous. I do not have problem with interlacing, resizer clock is lowered and there is no overlap between different video signals. CPU workload is ~50% and I get ~12 frames per second (4ch D1) with dm365. I can send short video as example and I am hoping that someone can help me.
Gradimir.