Hello, all.
I use DM388IPNC-IMX185, IPNC RDK VERSION 03.80.00.07 (FULL FEATURE) and a standard sample (ipnc_rdk_mcfw.out).
I need to get the raw image from the sensor.
I set in a file Rules.make two fields:
CAPTURE_DISPLAY_MODE_ON: = YES and FRAMES_TO_A8 = RAW.
When you load FS I see an error in the terminal window:
[m3vpss] 3131: Assertion @ Line: 848 in links_m3vpss / display / displayLink_drv.c: status == FVID2_SOK: failed !!!
In addition to these fields, no other changes were made.
What am I doing wrong?
Thank you very much.