This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DVSDK download for DM365/DM368

Other Parts Discussed in Thread: LINUXDVSDK-DM36X, OMAPL138, TMS320DM365, OMAP-L138, DM3730

I am start development for a DM365/Dm368 processor.  I am looking for the proper DVSDK to download.  

The "Get Software" button for this page  (http://www.ti.com/tool/LINUXDVSDK-DM36X)
 directs me to a general download page for then TMS320DM3730 DVSDK & OMAPL138 DVSDK. 

The DM365 or DM368 is not on this page.  Can someone direct me to the proper download for this processor?

  • Hi ,

    There is words saying This is the Generally Available (GA) release of the Linux DVSDK version 4. Supported processors are TMS320DM365/368, OMAP-L138, and TMS320DM3730/25.

    I would suggest you download it first and check if there is DM36x inside.

    BR,

    Eason

  • Thank you for the reply. 


    I installed the package on Ubuntu 10.04.  I ran into problems with a newer version of ubuntu. The install went smoothly.

    I see the DM365/DM368 folder and files installed with installer.  The Software developers guide describes setting up the environment for DM3730.  It also creates a Target File system and Linux Kernel for the DM3730.   I assume this is not compatible with DM365/DM368.  Is there a process for creating the DM365/DM368 Target kernel and file system?

    Thank you

    Joe Despirito

  • I found this page for the DM365/368

    http://processors.wiki.ti.com/index.php/GSG:_DVEVM_Software_Setup_for_DM3xx_Platforms

    Can  the procedure for build from this page apply?

    Joe