Hi, we would like to use DM385 for our video capture device which can support h.264 encoding which can reach 60fps at 1920x1080. I would like to ask the following question:
1) There is a HDMI TX in DM385. Can I bypass video input signal to that HDMI TX output directly? Since our product has one HDMI input and a HDMI bypass output (Signal from HDMI input).
2) There are three speed grade - (720-MHz ARM, 290-MHz HDVICP2), (970-MHz ARM, 410-MHz HDVICP2) & (1000-MHz ARM, 450-MHz HDVICP2). Which one I should use if I need 60fps h.264 encoding at 1920x1080.
Thank you!
Steve