Hello dear colleаguеs,
I connected a 3G modem (quectel uc20) on my custom DM365 board via USB hub (USB2517i). The kernel is 2.6.37 (PSP 3.21.00.04). Modem uses the "option" driver and creates five virtual serial ports (ttyUSB0 .. ttyUSB4) and works properly. But when I disconnet the modem, an error message loops forever:
"option: option_instat_callback: error -71"
I tried some different cases:
If I connect the modem via a second USB hub, the same error loops for a while and kernel continues with disconnection of the serial ports.
If I connect a second 3g modem , there is no error after disconnect the second one.
I also send the debug messages (debug level 8) from musb_hdrc while connecting/disconnecting the modem.
The logs are via second usb hub so error loop is not forever.
Please help me with this problem.
Best regards
Sunay