Hardware is DM368, software is Appro IPNC SDK 4.x
We have found an issue when setting bitrates >4Mbit for the 2nd stream in dual-streaming mode, the streaming just stops (no error messages) which then blocks the IPC queues and the whole thing stops responding.
I suspect it's to do with the bitrate being too high for the video data being generated - for example we can crash it easily by setting dual H.264 720p + QVGA and stream 2 bitrate ~4Mbit/s, lower bitrates it works OK.
Is there some formula I can use to calculate what the maximum sensible / allowable bitrate should be for a given resolution/framerate, or is there somewhere in the SDK I can gather debug information on what's going wrong?
It crashes when changing bitrate on the fly, or when starting up with a "bad" bitrate set.