Hi All,
HW: DM388 IPNC, BH XDS560V2 USB System trace Emulator
SW: CCS 5.3, IPNCRDK 3.8
I need to connect to video m3 of DM388 through CCS. Earlier , I have connected to DM816x EVM through CCS successfully.
1. There is no target config file for DM388 in CCS. Hence I used DM385 target config file
2. I am using IPNC_A8_DDR3.gel obtained from ipnc rdk_3.8
When connecting to A8, I am getting the below error.
CortexA8: GEL Output:
Connecting Target...
CortexA8: Output: **** DM385 ALL ADPLL INIT IS In Progress .........
CortexA8: GEL Output: SABERTOOTH ADPLLJ CLKOUT value is = 600
CortexA8: GEL Output: L3 ADPLLJ CLKOUT value is = 200
CortexA8: GEL Output: DSS ADPLLJ CLKOUT value is = 200
CortexA8: GEL Output: ISS ADPLLJ CLKOUT value is = 200
CortexA8: GEL Output: IVA ADPLLJ CLKOUT value is = 266
CortexA8: GEL Output: USB ADPLLJ CLKOUT value is = 192
CortexA8: GEL Output: VIDEO-0 ADPLLJ CLKOUT value is = 250
CortexA8: GEL Output: VIDEO-1 ADPLLJ CLKOUT value is = 148
CortexA8: GEL Output: VIDEO-2/HDMI ADPLLJ CLKOUT value is = 148
CortexA8: GEL Output: DDR ADPLLJ CLKOUT value is = 400
CortexA8: GEL Output: AUDIO ADPLLJ CLKOUT value is = 200
CortexA8: Output: **** SATA0 PLL INIT IS In Progress Please wait .....
CortexA8: Output: **** SATA0 PLL INIT IS In DONE *****************
CortexA8: Output: **** SATA1 PLL INIT IS In Progress Please wait .....
CortexA8: Output: **** SATA1 PLL INIT IS In DONE *****************
CortexA8: GEL Output: CONFIGURE PRCM CLOCKS of EMAC in progress
CortexA8: GEL Output: PRCM CLOCKS of EMAC is complete
CortexA8: Output: **** DM385 ALL ADPLL INIT IS Done **************
CortexA8: GEL Output: **** Configuring DDR PLL to 400 MHz.........
CortexA8: GEL Output: DDR ADPLLJ CLKOUT value is = 400
CortexA8: GEL Output: DM385 DDR3 EVM EMIF0 configuration in progress.........
CortexA8: GEL Output: DM385 DDR,DMM PRCM configuration is Done
CortexA8: GEL Output: DM385 DDR PHY Configuration is Done
CortexA8: GEL Output: DM385 DDR IO Control Configuration is Done
CortexA8: GEL Output: DM385 VTP Configuration is Done
CortexA8: Trouble Writing Memory Block at 0x4e000040 on Page 0 of Length 0x4: (Error -1065 @ 0x3D5A) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.402.0)
CortexA8: GEL: Error while executing OnTargetConnect(): Target failed to write 0x4E000040 at *((unsigned int *) (0x4E000000+0x40))=(unsigned int) 0x80600100 [IPNC_A8_DDR3.gel:201] at cmd_DDR3_EMIF0_Config(0x30, 0x21, 0xC0, 0x44, 0x00173208, 0x110B783B, 0x20437FDA, 0x501F86AF, 0x00000C30, 0x61C011B2) [IPNC_A8_DDR3.gel:2322] at DDR3_Init_400MHz_Config() [IPNC_A8_DDR3.gel:2295] at DDR3_Initialization() [IPNC_A8_DDR3.gel:1008] at OnTargetConnect() .
Any help would be greatly appreciated
Best Regards
JK