Hi,
my customer wants to replace TMS320DM368ZCED48F instead of TMS320DM368ZCED.
Is TMS320DM368ZCED48F fully compatible with TMS320DM368ZCED? Or firmware should be edited?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
my customer wants to replace TMS320DM368ZCED48F instead of TMS320DM368ZCED.
Is TMS320DM368ZCED48F fully compatible with TMS320DM368ZCED? Or firmware should be edited?
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/t/265326
48 stands for the higher speed grade, and F is face detection.
I think they are compatible. However, to enable the face detection, the firmware need to be changed.
BR,
Eason