Hi,
I am using IPNC RDK 5.1.0 and DM365 EVM. I want to display data on LCD.
1. Will it be possible using V4L2? As I can see the RDK is not having the Davinci Encoder Manager which is present in the SDK. Should that be an issue?
2. I want the data to be output in PRGB 888 format. For that I have set the required registers of VENC and OSD in the Video Encoder of VPBE? Should that be enough? As I can see the davinci fb file is not being compiled. Will that be required?
We do not have the LCD yet but when I boot the board with this uImage and run the moduletest for drv_display, I cannot see any signals on the LCDout lines on probing there. I have set the pinmux correctly for all 8 R, G and B lines.
Please guide me on what I should do to get the LCD display working. I can display composite on TVOUT just fine.
Regards,
Charvi.