Is there any information avaialble on the power consumption of DM38x devices? In particular I'd like to comapre against DM368 performing dual SD encode.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any information avaialble on the power consumption of DM38x devices? In particular I'd like to comapre against DM368 performing dual SD encode.
Thanks
Hi Eason,
1x H.264 576i encode
1x H.264 576i MJPEG Encode
VPSS enabled
ARM 70%
EMAC disabled
Case temp 25 deg C
Everything else disabled
If you need other details or the ones above aren't appropriate, pick them as you choose and let us know what the use case was.
Regards,
John
Hi Eason,
Thanks for this. I'm surprised. Since this is a next generation part I was expecting it to be lower. This looks like it will use more power than the DM8147, though I'm not sure how much the MJPEG-5 is consuming. A figure for 2x D1 encode only would really help.
Is a power estimation spreadsheet planned, as for other devices?
Regards,
John