HI - I have a Leopard board camera (3rd party standard product, built using a DM368) which drops frames - running at 720p60 i.e. 60fps 1280x720 resolution. On simple scenes it does not drop frames, but on complex scenes a few % of frames can get dropped. I think the system cannot finish the tasks in a single frame-time. What variables could I change to mitigate this? I'm only using the OSD for timecode-in-picture, and the video stream is just being saved directly to and embedded SD card
Are there services I can turn off that are consuming compute power? maybe face recognition or motion detection or ??
Can I switch to VBR from CBR encoding?
is there a way to easily go grayscale that would reduce processing, or is there a way to crop the image by a few% to reduce the task.
I'm thinking the product is essentially just a reference design from TI.
This is an urgent problem and we need help!
John G