I work with DM385 platform now.
When I create a capture-display chain to get the date from the VIP port ,it turns error with RGB888 dateformate into YUV422.
I wonder wheather VIP can transfer RGB888 into YUV 422 or not ?
regards,
Yang.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Brijesh Jadav.
1.
Sorry for my careless, I was then trying to figure it out. So I've change the parameters .
I want to get RGB input and YUV output.
Generally speaking , I want to capture the RGB888 date from the VIP port ,and display it .
According to my research these days ,I find that it could be done weather through VIP csc to converte RGB888 into YUV inside the VIP block,
or use the GRPX block to display the RGB888 date without change it . I got it from the blow picture.
But I have not seen a example of GRPX block . So I want to converte RGB888 to YUV through VIP csc block.
Now , we haven't prepare the external device to provide the RBG source. I want to get DM385 just ready to do that.
2.
I have hdvpss drivers ,then I would try .
Regards,
yang