Under DM365 and dvsdk_2_10_01_18 (Montavista 5.0)
I Tested Jpg rotation function with image_encode_io1 (image_encode_io1_dm365.x470MV), and it worked good. (The rotation function is implemented by myself).
But Under DM368 and dvsdk-evm_4_02_00_06 (CodeSourcery)
I used the same way to implement jpg rotaion, and the image_encode_io1_dm368.x470MV is blocked at IMGENC1_process()
I migrated dvsdk-evm_4_02_00_06's dmai to dvsdk_2_10_01_18, and the rotation function still workd good.
I think the cause is the difference between codec-engine_2_26_02_11( dvsdk-evm_4_02_00_06) and codec_engine_2_24 (dvsdk_2_10_01_18) .
But i can not find the prolem.
Is there any advice?
thanks