I am currently prototyping a portable camera using the following components:
2 Camera Boards from Leopard Imaging
1 TI DM 385 DaVinci Processor
1 TI WiLink WL1837MOD WIFI and Bluetooth Module
1 TI TLV320AIC26 Audio Codec
1 TI TPS65911 Power Management IC
1 Li-Ion Polymer Battery
Once the user presses a button the camera is powered up and should immediately start to stream the two video signals using the WiLink Module. How many seconds will pass until the camera is ready to transmit the video signals?
I do not need an exact calculation of the cameras start up time. All I need is a rough estimate how many seconds will pass until the camera is ready to stream the video signals. Will that be in a range of 1 or 2 seconds or in the range of 10 – 20 seconds?