In the VPFE manual, sprufg8c.pdf, page 457, section 6.6.5, there is a description for the Interrupt Selection Register.
Table 6-309 has the field descriptions.
For INTSEL3, it says a value of 15 is reserved. These values are used for INTSEL1 and INTSEL2 in different bit positions.
What does value 15 correspond to? It is used in the reference code (vpss.c) as the selection for INTSEL2.