With DM368,
Is it possible to capture (not encoding) 1080p 60fps video (16-bit sensor)?
What is the maximum fps with 1080p?
Regards,
Hayden
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
With DM368,
Is it possible to capture (not encoding) 1080p 60fps video (16-bit sensor)?
What is the maximum fps with 1080p?
Regards,
Hayden
Hi Hayden,
According to the TMS320DM36x Video Processing Front End (VPFE) section 1.2.1 Image Sensor Interface (ISIF) the maximum pixel clock could not exceed 120 MHz which means that it is not enough to capture 1080p@60fps.
BR
Tsvetolin Shulev