I am working with dm6446, everything is proper,
printenv is ok..., tftp is loading uImage_dm6446 ok...,
but when I am trying to boot using bootm command sending DHCP and RARP requests...ok, got DHCP answer from 0.0.0.0, my addr is 192.168.1.5
with the following message:
looking up port of RPC 100003/2 on 0.0.0.0
portmap: server 0.0.0.0 not responding, timed out
Root-NFS: unable to get nfsd port number from server, using default
Root-NFS: unable to get mountd port number from server, using default
mount: server 0.0.0.0 not responding, timed out
Kernel panic - not syncing: VFS: unable to mount root fs on unknown-block(2,0)
How to solve the above mention error messages....
I even checked the firewall its status is inactive and also restart the nfs-kernel-server before booting the board.
Can any one please help me with the above.
Regards
Jheel Shah