Hi all,
We are currently working on a project which has following requirements to meet:
- Capture raw video from HDMI of 1920x1200 resolution @ 30 fps
- Stream the video with h.264 encoding over Network (UDP/RTP) of 1920x1200 resolution @ 10 fps
- Store the video with h.264 encoding on local storage (SD card/USB) in .mp4 file with 1920x1200 resolution @ 10 fps
- Timestamp watermarking on streamed as well as stored videos
Currently we are using Z3 technology's Z3-DM368-VI-RPS kit for proof of concept.
The kit has 256 MB of RAM and 128 MB of on-board NAND flash.
Is it possible to implement above listed requirements with DM368 platform ?
biggest concern is that streaming and recording should be run simultaneously. Is it possible on DM368 platform ?
Thanks in advance.