Hi,
I am using DM365 processor with WinCE. I am trying to expand video 736Wx576H vertically in 420 format in VPBE with ratio (6/5). VideoWindow0 is used for Y and Video1 is used for C. In memory: Y data are first, after that follows C data. When I try to set VVRSZ=1 (BIT11) in MODE (vpbe OSD) register, I can get expansion 6/5, but the colours are misplaced. It looks like window1 was scaled with a higher ratio. Please can you confirm that the expansion should work in this scenario? If so, can you advise what else I need to check in registers settings?
Thank you.