I have a working system with a DM355 processor and now I want to do a migration to a DM365. The problem is that I didn't build up the existing software by myself but rather only was given the existing source code. What are the necessary steps, regarding the software, to come out with an updated system that at the end of the day has the same behavior but a different processor, namely a DM365 instead of a DM355? My first approach was to change the base addresses in the memory with respect to the respecting memory maps but it didn't work...Thank you in advance.