Hello,
Just wondering if you have a schematic examples or Development kit where the video processor used with a MIPI CSI-2 to Parallel port bridge device.
our OVM9724 request a bridge device to transfer the data to DM368
Thank you
Dino
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Just wondering if you have a schematic examples or Development kit where the video processor used with a MIPI CSI-2 to Parallel port bridge device.
our OVM9724 request a bridge device to transfer the data to DM368
Thank you
Dino
AFAIK, DM36X supports only 16-Bit Parallel AFE (Analog Front-End).
HI,
As said in above post, I am unaware if DM365/DM368 supports MIPI (I doubt that). However, DM38X family of devices do supports MIPI.
Referring to page-34, DM365 supports only 16-bit parallel interface.
Please can you share the link or reference of any data sheets which says MIPI supported on DM365? That will help us.
Thanks
I totally agree that that DM365 and DM368 doesn't support MIPI, may question is there an interface a bridge for that propose. I looking for something like the TC358746AXBG from toshiba it's a MIPI CSI-2 to Parallel port and Parallel port to CSI-2.
TC358746AXBG is a bridge device that converts MIPI data transfers from devices such as a camera to an application processor over a Parallel port interface.
I just looking to see if I'm in the right direction, or there is similar parts that TI may have for this purpose.
Thank you again
Dino
Ravikiran,
Thank you for your response,
I'm trying not to use the bridge I have selected previously due to lack of support. Does TI have a conversion bridge that fit for this application.
Thank you again
Dino