Tool/software: Linux
Hello,
We have Spectrum DM368 EVM & IPNC RDK v 5.1.0.
We want to port the IPNC application on the EVM. In the IPNC user guide document, we have seen that IPNC RDK can be built for evm by changing the rules.make file.
We have also checked av_server application. In this application, some gpios are used for alarms, SD Card Detect, SD Card Protect. But in DM36x EVM same Gpios are used for different purposes.
We have following queries
1. Is it possible to run the same applicaiton on DM36x EVM or need to update the application? If update required, then what changes will be required?
2. Can we boot the EVM using SD Card? If yes, then what changes required?
Regards
Uma Shanker