This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DM388
Tool/software: Code Composer Studio
Following are the problems faced with TMDSCSK388;
i. CCS Issue (on Windows): CCS 7.1.0 is installed in the system. DM388 CSK Hardware diagnostics project obtained/downloaded from Ti, is imported into CCS. While configuring the target we are unable to find DM388 nor TMDSCSK388 from board or device list.
ii. Boot Up Issue : Based on the user guide, the TMDSCSK388 is set up. Unable determining Board IP Address . In TeraTerm after setting the serial port option, Boot up is not happening its showing " CCCCCCCC " continues in tera term window. No boot up and not getting RTSP links. The SD Card received along with the board is inserted in the card slot.
iii. Boot Up with New SD card: The prebuilt binaries from the IPNC RDK 3.9.0 package is flashed on the new micro-SD by followed the Prepare SD Card steps form Boot Setup for CSK. Replacing the SD card received along the board with new SD card did not solve the issue, no boot up with new SD card also.
I request you to support me to resolve above issues
Hi,
For the 1st Issue you can select the target as ti814x.
For the other 2 issues, i will check with my team and let you know.
Reagrds,
Anuj
Regards,
In reply to Anuj Kumar Gupta:
Thanks and Regards,
Dwarakesh R.
PathPartner Technology
-Ravikiran
Please close the thread by clicking "verify answer" button, if this answers your question.
In reply to Ravikiran HV:
In reply to Johnson Geo:
Hi Ravikiran,
I'm unable to get any FAE contacts. I kindly request you to provide help asap.
Thanks
Hi Johnson Geo,
I have forwarded this query to to concerned person. Awaiting for the response before I share the details.
Meanwhile please can you answer above question?
AFAIK, TI ccs project for csk is not part of ti release. Please can you share the download link ?