Hi Ti:
We have completed porting of AR0521 sensor on dm388.
We meet a problem that image has strange line at right side.
I have no idea about it.
And the image is normal in 1080p resolution (1920 x 1080)
And our sensor 5M output is 2592 x 1944.
But TI DM388 5M can only set to 2560 x 1920.
I am not sure if it is the root cause.
Our 5M settings is below.
/ * Camera Link params */
CameraLink_CreateParams_Init(&cameraPrm);
cameraPrm.captureMode = CAMERA_LINK_CAPMODE_ISIF;
cameraPrm.outQueParams[0].nextLink = dup5MId ;
cameraPrm.outQueParams[1].nextLink = dupVGAId;
cameraPrm.numAudioChannels = 0;
cameraPrm.numVipInst = 1;
cameraPrm.tilerEnable = FALSE;
cameraPrm.maxWidth[0] = 2560;
cameraPrm.maxHeight[0] = 1920;
cameraPrm.maxWidth[1] = LCM_WIDTH;
cameraPrm.maxHeight[1] = LCM_HEIGHT;
/* setup sensor output */
cameraPrm.vsEnable = 0;
pCameraInstPrm = &cameraPrm.vipInst[0];
pCameraInstPrm->vipInstId = SYSTEM_CAMERA_INST_VP_CSI2;
pCameraInstPrm->videoDecoderId = MultiCh_getSensorId(gUI_mcfw_config.sensorId);
pCameraInstPrm->inDataFormat = SYSTEM_DF_BAYER_RAW;
pCameraInstPrm->sensorOutWidth = 2560;
pCameraInstPrm->sensorOutHeight = 1920;
pCameraInstPrm->standard = SYSTEM_STD_5MP_2560_1920;
pCameraInstPrm->numOutput = 2;
/* First stream */
pCameraOutPrm = &pCameraInstPrm->outParams[0];
pCameraOutPrm->dataFormat = SYSTEM_DF_YUV420SP_UV;
pCameraOutPrm->scEnable = FALSE;
pCameraOutPrm->scOutWidth = 2560;
pCameraOutPrm->scOutHeight = 1920;
pCameraOutPrm->standard = SYSTEM_STD_5MP_2560_1920;
pCameraOutPrm->outQueId = 0;
/* Second stream */
pCameraOutPrm = &pCameraInstPrm->outParams[1];
pCameraOutPrm->dataFormat = SYSTEM_DF_YUV420SP_UV;
pCameraOutPrm->scEnable = FALSE;
pCameraOutPrm->scOutWidth = 320;
pCameraOutPrm->scOutHeight = 240;
pCameraOutPrm->standard = SYSTEM_STD_VGA_60;
pCameraOutPrm->outQueId = 1;
DarkHou