Hi ,
I have two frames coming in to Sw mosaic is there any way to scale one of the input by configuring sw mosaic parameters?
I have two inputs to Merger , How the two inputs are arranged as single output?
My sw mosaic is going to configure 2 layouts in this case, How the mosaic link knows which of the buffer from the combined buffer output of merger should go to win0 and which one to win1?
1------>
merger ----------------------------------------------------------------------> swmosaic(w0 and w1) -----------------------------------------------------------------------------------> display
(how they are arranged) (which one is linked with win0 and which one with win1)
2------->
thanks
Kailash