hi,
I'm using IPNC_RDK 3.9.0, In this I'm trying to understand the function call of Void CameraLink_tskMain(struct Utils_TskHndl * pTsk, Utils_MsgHndl * pMsg);
in ipnc_rdk-3.9.0/Source/ipnc_rdk/ipnc_mcfw/mcfw/src_bios6/links_m3vpss/camera/cameraLink_tsk.c
If my undestnding is correct it is called by
.............................
status = Utils_tskCreate(&pObj->tsk,
CameraLink_tskMain,
CAMERA_LINK_TSK_PRI,
gCameraLink_tskStack,
CAMERA_LINK_TSK_STACK_SIZE, pObj, "CAMERA ");
.................................
in Int32 CameraLink_init()
if that is the right way, I'm trying to call CaptureLink_tskMain(); in ipnc_rdk-3.9.0/Source/ipnc_rdk/ipnc_mcfw/mcfw/src_bios6/links_m3vpss/capture/captureLink_tsk.c
But the function is not called.
I notice
/** Create link task, task remains in IDLE state
CameraLink_tskMain is called when a message command is received
*/
How I can make a message command available for capture.
All Helps and advices are appreciated
Thank you
Regards