Hi Champs,
In a view of a IP camera project I have the following questions :
Q1 : We are looking for a global dynamic range sensitivity close to 120dB. Do you have numbers in term of dynamic range sensitivity on a DM TMDSCSK board + camera sensor? Could we reach such target with DM HW ISP HDR module ? (for DM388 and DM81XX)
Q2 : Are those sensors compatible with DM388 and DM81XX
- Gamme Starvist de Sony : IMX123 ou IMX290 ?
- OnSemi : AR0331 (it sounds like it is supported)?
- OmniVision : OV2732, OV4689 ?
Thank you
BR,
Guillaume