Hello,
We are using DM388 CSK and IPNC 3.9.1 . We want to use blending feature in DM388 CSK IPNC.
But as per OSD User Guide Document, blending feature is not supported by DM388 IPNC.
Please let us know the following:-
1. In DM388 IPNC 3.9.1, blending is supported or not?
2. If not, then when it will be available?
3. If availability of blending feature in IPNC is so far, then can we develop the Blending feature. If yes, then what are the steps we have to follow.
Regards,
Uma Shanker