Tool/software: Linux
we use the DM385 and IPNC RDK3.91.
We use ADV7611 to connect to dm385's vin[0].We are going to create and open the capture link in the demo, but there is a problem during the creation process.
The error message is as follows:
[m3vpss ] 2428: CAPTURE: Create in progress !!!
[m3vpss ] 2465: CAPTURE: VIP0 PortA capture mode is [16-bit, Non-mux Discrete Sync - HSYNC_VSYNC] !!!
[m3vpss ] 2465: Assertion @ Line: 667 in links_m3vpss/capture/captureLink_drv.c: pInst->captureVipHandle != NULL : fail
The error function is as follows:
pInst->captureVipHandle = FVID2_create(FVID2_VPS_CAPT_VIP_DRV, pInst->instId, pVipCreateArgs,&pInst->createStatus, &pInst->cbPrm);
Our changes here:
1. In the multich_tristream_fullfeature.c added capturelink incoming parameters and create functions.
2.Mask the function about the camera.
This problem is always not solved. Please give me some suggestions. Thank you!