Hi,
I have a problem with the dm355 demo. When i run the demo for the first time the output coming from the tv out was black and white.
After some changing in the boot menu i obtained the tv out signal with color, but when i rebooted the dm355 the demo has black and white output.
By the way the encode+decode demo can't run when my input is a color camera.
I think it can be a dm355 hardware problem. What do you think?
Here there is my printenv:
>DM355 EVM # printenv
>bootdelay=3
>baudrate=115200
>bootfile="uImage"
>nfshost=192.168.1.2
>rootpath=/home/workdir/filesys/target
>filesize=183098
>fileaddr=80700000
>ipaddr=192.168.1.3
>serverip=192.168.1.2
>bootcmd=nboot 0x80700000 0 0x400000; bootm
>bootargs=console=ttyS0,115200n8 noinitrd ip=192.168.1.3:192.168.1.2:192.168.1.1:255.255.255.0:::off root=/dev/mtdblock3 rw rootfstype=yaffs2,nolock mem=116M'
>stdin=serial
>stdout=serial
>stderr=serial
>videostd=pal