Hi,
I've been given the task of reinstalling the montavista linux distribution onto a DM355 EVM board, after another individual installed Windows CE 6 on it.
I have tried using the TI application DVFlasher_1_10.exe, but it appears to not complete its transaction when I try and sent u-boot-1.2.0-dm355_evm.bin.
Below is the console output:
-----------------------------------------------------
TI DVFlasher Host Program for DM644x
(C) 2007, Texas Instruments, Inc.
-----------------------------------------------------
Platform is Windows.
Restoring NOR flash with u-boot-1.2.0-dm355_evm.bin.
Attempting to connect to device COM1...
Press any key to end this program at any time.
Waiting for DVEVM...
DVEVM: BOOTME
BOOTME commmand received. Returning ACK and header...
ACK command sent. Waiting for BEGIN command...
DVEVM: BEGIN
BEGIN commmand received. Sending CRC table...
CRC table sent. Waiting for DONE...
DVEVM: DONE
DONE received. Sending the UART UBL file...
DVEVM: DONE
DONE received. UART UBL file was accepted.
UART UBL Transmitted successfully.
It then continues to sit here as if waiting for another command from the target.
I found a thread on another site dated in May 2008 that there would be a DVFlasher application for the DM355 released very soon - is this available yet, considering it is August now?!
Michael