The release notes for the LogicPD Linux BSP for the Torpedo say that it has no camera support, which is required for my application. I don't understand this since there are drivers for a number of CPI devices in other kernel versions for the DM3730 (including the DVSDK), so why would they be missing from this kernel? I see at least some of the code for these drivers in the LogicPD kernel source and if I try to use one of them (e.g. modprobe mt9v022), the module loads but doesn't appear to do anything (no kernel messages). I know from what I've read that there are other pieces needed to make the driver work (bridge driver, CCDC driver, u-boot parameters) - the details are not clear at all to me yet - and I assume that some of these are disabled or missing.
What if I were to try to use the DVSDK instead of the LogicPD BSP? Would it work with the Torpedo?
Any comments or insights would be appreciated.
Thanks,
Mike