I use linux-2.6.37 from DVSDK-4.6
I have camera OV5640.
And I can get image from this pipeline:
Sencor->CCDC->MEM
But I can't get image when pipeline:
Sensor->CSI2a->MEM
I compared implantation of omap3-isp driver from linux-2.6.37 and linux-3.11.
In linux-3.11 csiphy configuration is different.
I modify implementation csiphy(linux-2.6.37) like in linux-3.11.
But image can't be capture. Any CSI 2 interrupts doesn't occur
What I need to do to capture image via CSI2?