Hi All,
We are using VAR-SOM-OM37 SOM(DM3730 + TPS65930) from variscite with kernel version 2.6.37 and Gingerbread android OS.
I am facing some power consumption issues with Wi-Fi during suspend state.
- If we won't enable WI-FI, The SOM current consumption is ~6mA and Wi-Fi module consumption is 0mA.
- But if i enable Wi-Fi and suspends the device, The SOM power consumption is very high ~40mA(Continuosly). But the Wi-Fi is consuming only 0mA except while it is scanning for routers.
We connected Wi-Fi I/F to MMC2 controller. I am not handling OMAP SDIO pins during suspend.
I need this very urgently as we are going to deliver our product. So can anyone please help me on this?
Thanks,
Naresh