Hi
I am using the media-ctl framework and would like to do the resizing. Previously, using the Resizer code from TI works perfectly on dvsdk4.02 where it looks for /dev/omap-resizer and does the resizing on the evaluation board. But I'm using the OMAP3 ISP resizer, I changed the /dev/omap-resizer to take in /dev/video5. It didnt work as expected. Is there some workaround or any solutions?
Would fwrite into /dev/video5 and fread from /dev/video6 works?
Please help. Thanks.
- entity 10: OMAP3 ISP resizer (2 pads, 4 links) | |
type V4L2 subdev subtype Unknown | |
device node name /dev/v4l-subdev4 | |
pad0: sink [fmt: UYVY2X8/720x480 crop.bounds:(0,0) crop:(0,0)/720x480] | |
<- 'OMAP3 ISP CCDC':1 [] | |
<- 'OMAP3 ISP preview':1 [] | |
<- 'OMAP3 ISP resizer input':0 [ENABLED] | |
pad1: Source [fmt:UYVY2X8/320x240] | |
-> 'OMAP3 ISP resizer output':0 [ENABLED] |