Hello,
I have compiled a project in IAR (uc/os) and it is in out format.
I see in map various address as following:
...
__vector 0x80000000 Code Gb cstartup.o [1]
_call_main 0x80000ae4 Code Gb cmain.o [5]
_exit 0x80000bd4 Code Gb cexit.o [5]
_main 0x80000aec Code Gb cmain.o [5]
exit 0x80000ba1 0x4 Code Gb exit.o [3]
main 0x80000b30 0x68 Code Gb app.o [1]
...
Now I try to load it into running u-boot, but it seems not to work, I'm not sure why.
I first tried to do the conversion as following:
out->hex->img (kmimage) and load with :
loadb 0x80000000
go 0x80000000
Is that correct ? Will it put the symbols in the correct addresses ?
Thanks for your help,
Ran