Hello,
We are using the specified device (DM3730CUSD100) in our application.
Looking at table 3-3 under the OPP130 col for 105C there is no information available, do you have any?
We might have a case where we use the industrial component with junction temperature exceeding 90C (Lets say 92-95C for short time periods - seconds), do you know if the possible damage to the life time of the device is addative? (Other way to ask it if the device only partially works at high junction temperature what are the risks?
Is table 3-3 valid for the extended temperature range or only for the industrial?
Should I worry about using the industrial devices for few seconds at ~95C?
Another question is what is the difference between the extended temp range and the industrial devices? Is it produced in the same line and the difference is tests only?
Thank you.