Other Parts Discussed in Thread: TMS320C6747
I have apiece of code for enabling and writing GPIO and blink LED. This code is working fine in OMAPL137 board with TMS320C6747 core. When same is tried in TMS320C6745 processor (One board I ve designed), it is not working. It is not writing to the memory assigned for GPIO.I ve used the default GEL file for OMAPL137 & TMS320C6747. But not working in both. I dont have GEL file for 6745. . But I am able to connect the 6745 board (which I ve designed) to CCS and able to debug and put preak points. So only GPIO related stuff is not working.Please help me