All,
I am excited to announce that thanks to our a long term relationship with Microsoft, we have developed a high performance embedded software version of the RemoteFX protocol which is released today on over 300 Millions PC with windows 7 SP1.
This implementation runs today on the DSP integrated on DM3730 and provide RemoteFX decode capability up to 1280x1024 at minimum 24fps.
You can see the HP thin client Team demonstrating their DM3730 based system at Tech Ed last November, at the following link : http://www.youtube.com/watch?v=46bi-j_KzCQ
The big innovation here is that RemoteFX encodes on the server side from the graphic card , it means,any kind of windows, 3D graphics effects or videos can be encoded as you would see it on an real desktop, and so the thin clients using RemoteFx will render ALL features of your desktop / Server, This is a first !!!
You can see Nara , our engineering manager demonstrate the capability of DM3730 in this video : http://www.youtube.com/watch?v=zR0Ij44srnE
We are also working right now on our next generation DM part that will enable dual screen experience from a single thin client box for professional market, this with higher resolution and higher frame rate !!
You can also go to microsoft blog at : http://bit.ly/RemoteFX for more information on RemoteFX.
Best Regards,
Jean-Marc Darchy
C6000 Advanced Displays