• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors » DM37x DaVinci Video Processor Forum » All Tags » AM3730
Share
DaVinci™ Video Processors
  • Forums
  • Announcements

Browse by Tags

DaVinci™ Video Processors

Welcome to the DaVinci™ Video Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
AM3730
  • AM/DM3730
  • beagleboard
  • Beagleboard-xm
  • bootloader
  • Camera
  • Camera ISP
  • CCSv4
  • DaVinci
  • DM3730
  • DM3730 screen
  • DM3730 Beagleboard camera
  • DM3730 data manual
  • dm3730 Linux
  • DM3730 Linux Kernel 2.6.32
  • DM37x
  • DM37xx
  • Flash Tool
  • GPMC
  • LCD
  • OTG
  • Power management
  • TI_Android_FroYo_DevKit-V2.2
  • TMDEXVM3730
  • u-boot
  • USB
Related Posts
  • Forum Post: Re: PROBLEM IN NAND FLASH WHILE RUNTIME

    Bhagavath Ram Bhagavath Ram
    Hi sir .. Thanks for your suggestion...But can you please describe how to do NAND flash on board ...what i m thinking is that package of stack is correct (AM3730) but my mistake in NAND flash step... Can u please tell this thing or else can you please send me Document for flashing ..... Regards...
    on Jul 21, 2011
  • Forum Post: Re: PROBLEM IN NAND FLASH WHILE RUNTIME

    Bhagavath Ram Bhagavath Ram
    Hi Vishveshwar Bhat. Thank for you are reply ... Nand boot is working fine ..then i have another issue... where the usb ll mount on the board..i plug the usb its show the below message but i cannot find out the path of usb in board.. How you can access the usb with android on AM3730 board usb 1...
    on Jul 21, 2011
  • Forum Post: Re: USB DMA DM37x

    Esaias Pech Esaias Pech
    Swami, Thank you for your answer, I'm guessing I should pay closer attention to the am35x.c right? So just to double check, 1. The AM37x uses the same CPPI DMA the OMAP L138 uses? 2. Is it the same offset as the OMAP L138? Thanks
    on Aug 22, 2011
  • Forum Post: USB DMA DM37x

    Esaias Pech Esaias Pech
    Hello, I am adding DMA functionality to a driver I wrote (driver is able to send/receive via Bulk transfers but not at the speed I need) I have a couple of questions: First question In the Beagleboard xM, the USB OTG Base address is 0x480AB000. What's the offset of the DMA registers...
    on Aug 21, 2011
  • Forum Post: Missing documentation for DM3730

    Esaias Pech Esaias Pech
    Hello, I have some questions regarding the documentation for the DM3730 microprocessor. 1. Which document should I follow to implement the USB DMA in this microprocessor , note that I said document and not driver in Linux (everyone seems to be pointed out to analyze the USB Driver to get the information...
    on Aug 24, 2011
  • Forum Post: Booting loader

    Bigtree Bigtree
    I am new to ARM and I am going to work on a new ARM development design using DM3730. Since my application is relatively small so I don't plan to use an OS. Then do I have to write the bootloader myself or I could get a bootloader code without OS. Also I will use Code Composer 4.x as SDK. Would the...
    on Sep 15, 2011
  • Forum Post: Re: DM3730 SDRC data strobe timing(DLL/CDL)

    Toshio Ushikubo Toshio Ushikubo
    Please someone post any response to my question. Regards.
    on Oct 13, 2011
  • Forum Post: DM3730 SDRC data strobe timing(DLL/CDL)

    Toshio Ushikubo Toshio Ushikubo
    Please answer following questions. Is the delay described below 90-degree which is adjusted inside DM3730? And if we'd like to enable that delay we have to set ADRC_DLLA_CTRL register as follows, don't we? SDRC_DLLA_CTRL = 0x0000000A means follows. FIXEDDELAY = 0 DLLMODEONIDLEREQ...
    on Oct 7, 2011
  • Forum Post: AM/DM37xx EVM driver library

    Bigtree Bigtree
    Hi Experts, My company purchased AM3703 EVM and support package for Linux, WinCE and Android. I installed Linux toolchain and supporting SDK package. But I could not find the driver library to configure for example DMA, GPMC or interrupts. At least there should be #defines for the hardware registers...
    on Oct 27, 2011
  • Forum Post: Kernel Panic Error

    Bhagavath Ram Bhagavath Ram
    Hi all, Here i am using TI_Android_GingerBread_2_3_4Sources android stack for omap3evm board , i have done some changes in lcd in android kernel ,then i tried to boot the board through SD card (4GB),its booting the kernel successfully ,after that its showing the log as shown below , kindly Please...
    on Jan 4, 2012
  • Forum Post: Images not seen on LCD with android kernel

    Bhagavath Ram Bhagavath Ram
    Hello ti, I am using TI_Android_GingerBread_2_3_4Sources android stack for omap3 based custom board with 7"inch LCD display , We are not getting anything on the LCD display ,but in the console the Android is booted. With the following changes in the BSP kerne(PSP release 4.0 .0) ,not...
    on Jan 5, 2012
  • Forum Post: Linux aware debugger for DM3730

    valeswararao d valeswararao d
    Hi all, I am looking for JTAG debugger for DM3730 which supports Linux aware debugging ( to debug Linux kernel). Please suggest me that which one is good for kenrel debugging and DSP-BIOS debugging (XDS100,XDS510,XDS560, lauterbach ).and have better support. Thanks & Regards Valeswara...
    on Dec 26, 2011
  • Forum Post: How to use camera port to transfer RGB data?

    peng xiao peng xiao
    Hardware D escribes : CPU DM3730 Camera Pin connections to FPGA D[0:11] I PCLK I HS I VS I CAM_WEN I I :means input Data from Camera interface through ISP, and the CPU get data from DMA ram. We don't need the ISP module to do any change the data from the camera interface....
    on Mar 6, 2012
  • Forum Post: MICRON MT46H64M32LFCM-6 IT / DM3730 Compatibility ?

    ozer senyildiz ozer senyildiz
    Hi, Does MICRON 2Gb 64x32 32 bit MT46H64M32LFCM-6 IT LPDDRAM works fine with DM3730 ? Thanks
    on Aug 8, 2012
  • Forum Post: RE: Support for DM3730 with SYS/BIOS in CCSv5

    Stephen Wells Stephen Wells
    I would be very interested in explicit support for AM3730 or DM3730 CortexA8 in SYS/BIOS. Or even documentation to illustrate how any variant can be added and built. Going through RTSC documentation and learning how to create components and use the XDCtools should not be required for CCSv5 projects...
    on Nov 5, 2012
  • Forum Post: Can't cross compile uboot or Linux under Ubuntu - /bin/bash: arm-arago-linux-gnueabi-gcc: command not found

    Elvin Wong Elvin Wong
    Hi, I'm using Beagleboard XM. I tried to compile the u-boot and Linux bundled inside ti-sdk-beagleboard-05.03.02.00. My Ubuntu is running under VMware with Windows XP host. when I've setup everything and installed the Sitara Linux SDK according to the user guide, I tried to compile the...
    on Feb 12, 2012
  • Forum Post: how to change core pll configure in dm3730 uboot(2010-12)

    gzz gzz
    i want to change core pll ,because linux kernel start:the clock display: 0.000000] Clocking rate (Crystal/Core/MPU): 26.0/332/600 MHz i want to change core pll to 664MHz so i change some configure in uboot prcm_init ,but no matter what i change,the kernel all displays the same data. i can't...
    on Mar 7, 2013
  • Forum Post: About "Internal error" generated by the pvrsrvkm driver

    Masanori Koseki Masanori Koseki
    Hello, If pvrsrvkm driver's insmod and rmmod are done, internal error is generated. If "devmem2 0x48004B48 w 0x2" is executed after insmod, and he or she does rmmod afterwards, the error generates the pvrsrvkm driver. "devmem2 0x48004B48 w 0x2" Processing is executed by...
    on Mar 26, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use