• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors » DM37x DaVinci Video Processor Forum » All Tags » DM37x
Share
DaVinci™ Video Processors
  • Forums
  • Announcements

Browse by Tags

DaVinci™ Video Processors

Welcome to the DaVinci™ Video Processors Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
DM37x
  • AM3730
  • android
  • beagle Board XM
  • Beagleboard-xm
  • C64x+
  • Camera
  • Camera ISP
  • Codec Engine
  • DaVinci
  • DaVinci DM3730
  • DM3725
  • DM3730
  • DM3730 screen
  • dm3730 Linux
  • DM37xx
  • DSP
  • Flash Tool
  • GPMC
  • Linux
  • NAND Flash
  • OMAP
  • omap3
  • Power management
  • u-boot
  • USB
Related Posts
  • Forum Post: DM3730 CUS PACKAGE GPMC PIN MULTİPLEX FOR SRAM CONNECTION

    ozer senyildiz ozer senyildiz
    Hi, My 1MB nvsram has 19 Adress bits but the dm3730 has only A1-A11 adress pins. And also A11 pin is indicated as N/A for CUS package as below in datasheet: I Does anyone knows what to do with gmpc_a11 pin ? On the other hand Could you please me help how to extend gmpc address pins to 19 ?...
    on Jun 29, 2012
  • Forum Post: USB DMA DM37x

    Esaias Pech Esaias Pech
    Hello, I am adding DMA functionality to a driver I wrote (driver is able to send/receive via Bulk transfers but not at the speed I need) I have a couple of questions: First question In the Beagleboard xM, the USB OTG Base address is 0x480AB000. What's the offset of the DMA registers...
    on Aug 21, 2011
  • Forum Post: Dual Cameras

    Dave Pulvermacher Dave Pulvermacher
    I am designing a schematic with the DM3730 DSP. I may need to connect two cameras to my board. I see in the specifications that this is possible utilizing SCCB (serial camera control bus) on the I2C ports. I see a max data rate of 100kbits/s for the SCCB interface protocol. Is that accurate? I am...
    on Aug 29, 2011
  • Forum Post: Booting loader

    Bigtree Bigtree
    I am new to ARM and I am going to work on a new ARM development design using DM3730. Since my application is relatively small so I don't plan to use an OS. Then do I have to write the bootloader myself or I could get a bootloader code without OS. Also I will use Code Composer 4.x as SDK. Would the...
    on Sep 15, 2011
  • Forum Post: Re: Prefetch abort on DM3730 Cortex-A8

    Norman Beyer Norman Beyer
    Hi Jeff, It turns out that the Quantum Platform QDK/C++ for GNU/IAR ports on the Quantum Leaps ( www.state-machine.com ) web site had the answer for implementing interrupts with the QP OS running on the Cortex-A8 on the DM3730 soc - and yes amongst some other items it requires running in System...
    on Sep 23, 2011
  • Forum Post: Audio stream between Arm to DSP

    Marco Moschetti Marco Moschetti
    Hi everyone, I'm new to the forum. We have our own custom DM3725 platform and we are developing a realtime audio application with very low latency requirements (musical instrument). So McBSP is directly driven by DSP that make most of the critical work. But we need also to have some audio work...
    on Sep 28, 2011
  • Forum Post: Re: DM3730 SDRC data strobe timing(DLL/CDL)

    Toshio Ushikubo Toshio Ushikubo
    Please someone post any response to my question. Regards.
    on Oct 13, 2011
  • Forum Post: Re: DM3730 SDRC data strobe timing(DLL/CDL)

    Toshio Ushikubo Toshio Ushikubo
    My customer has intermittent LPDDR read error and has following question. DM37x (SPRUGN4N) Technical Reference Manual ,"10.2.4.4.11 Controlled Delay Line"(page 2267) explains that DDL/CDL function and it says "The DLL output is a command that controls the CDLs (plus the controlled...
    on Oct 20, 2011
  • Forum Post: DM3730 SDRC data strobe timing(DLL/CDL)

    Toshio Ushikubo Toshio Ushikubo
    Please answer following questions. Is the delay described below 90-degree which is adjusted inside DM3730? And if we'd like to enable that delay we have to set ADRC_DLLA_CTRL register as follows, don't we? SDRC_DLLA_CTRL = 0x0000000A means follows. FIXEDDELAY = 0 DLLMODEONIDLEREQ...
    on Oct 7, 2011
  • Forum Post: AM/DM37xx EVM driver library

    Bigtree Bigtree
    Hi Experts, My company purchased AM3703 EVM and support package for Linux, WinCE and Android. I installed Linux toolchain and supporting SDK package. But I could not find the driver library to configure for example DMA, GPMC or interrupts. At least there should be #defines for the hardware registers...
    on Oct 27, 2011
  • Forum Post: Re: [u-boot] USB-Host: no clockout on HSUSB2_CLK (GPIO_24)

    Atul Kumar Atul Kumar
    Hi Fixed the issues with below patchs.. http://comments.gmane.org/gmane.comp.boot-loaders.u-boot/121877 Regards Atul kumar
    on Jan 17, 2012
  • Forum Post: DM3730 Problem/ Android 2.2

    Vivian Sun Vivian Sun
    Hi, Our customer is developing products based on DM3730, using Android 2.2 (TI_Android_DevKit 02_02_00), found the following problem when doing system power on/off testing. Have tested two products with 100 times power on/off (power on---wait for Android GUI showing on LCD -->power off-->power...
    on Dec 28, 2011
  • Forum Post: GPMC NAND driver software for bare-metal application

    Norman Beyer Norman Beyer
    Does anyone know of any third-party driver software for GPMC NAND on DM3730 or OMAP3530 Socs for a bare-metal application (no Linux or other OS)?
    on Feb 23, 2012
  • Forum Post: Trouble connecting to ARM on LogicPD DM3730 Torpedo Board from CCSv5.1

    Oscar Llerena Oscar Llerena
    Hello, I'm attempting to connect to the ARM on my LogicPD DM3730 Torpedo board from CCS v5.1, and am getting an error (see console output below). I'm using a Spectrum Digital XDS560v2 to connect to the board. I've downloaded and installed the DaVinci Device Support Files, v1.0.3...
    on Mar 23, 2012
  • Forum Post: SPI usage by DSP C64x (DM3730)

    Sergey Zavyalov Sergey Zavyalov
    Hi, Could pleas answer - is it possible to use SPI port from DSP side ( TMS320C64x+ ) at the board based on DM3730?
    on Apr 18, 2012
  • Forum Post: Linux version selection questions

    EugeneS EugeneS
    Our board which uses DM3730 has LS-Research wireless module(Ti-Wifi 1271) and vendor we are working with says that in order to operate this module in the AP mode we probably better start using Linux kernel 3.x. On the hand we depend on TI DVSDK's codecs server package for (video encode/decode...
    on Apr 19, 2012
  • Forum Post: Disadvantage of MIPI interface

    SathyaKumar SathyaKumar
    Hi all, I am able to differentiate the advantage of MIPI over parallel interface. Probably the speed, power, standardization and data rate are the general advantages of MIPI. But what can be told as disadvantage?
    on Sep 10, 2012
  • Forum Post: RE: MIPI serial camera interface support in DM3725

    SathyaKumar SathyaKumar
    Hi Rajesh, You can check out this http://www.e-consystems.com/MIPI-Camera-Board-AM-DM37x.asp link as the proof for implementation of MIPI on DM37x processor. Maybe this will help you. Regards, Sathya Kumar P
    on Oct 9, 2012
  • Forum Post: RE: MIPI serial camera interface support in DM3725

    SathyaKumar SathyaKumar
    Hi Rajesh, Ya you are right. CBP and CBC package provide support for CSI. Unfortunately, CUS package keeps those pins as Not-Connected. It is better to move on to the CSI supported package or else you can interface deserializer to the processor parallel interface pins. Regards, Sathya Kumar P
    on Oct 9, 2012
  • Forum Post: RE: Streaming h264 video from one DM37x to another DM37x

    Richard A Hendricks Richard A Hendricks
    The software used is LogicPDs 2.2-2 BSP based on Linux kernel 3.0. I am not sure which DVSDK we are incorporating, I will check with our software team to determine that. I do not think it is a loading problem. The streamer works fine, I can even tee to the display, and watch the stream from multiple...
    on Nov 21, 2012
  • Forum Post: RE: Is Camera ISP software driver available for DM3730?

    Prabu Kumar Prabu Kumar
    For converting the RAW to YUV ,there is a limitation on the horizontal size.Check the 6.4.7.1 section. "Horizontal averaging by a factor of 1, 2, 4, or 8 in the horizontal direction. The preview module can output a maximum of only 4096 pixels horizontally due to fixed memory-line sizes" ...
    on Apr 2, 2013
  • Forum Post: GPS 8100-S not working properly with DM3730

    Harshit Suri Harshit Suri
    Hello Everyone, I am using a DM3730 EVM (Embest's Devkit8500D) with a GPS module, GPS 8100-S. The module comes with a testing application that reads NMEA streams coming from the GPS module. Here is the code: #include <stdio.h> #include <string.h> #include <stdlib.h> #include...
    on Jun 7, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use