• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors » DM814x and AM387x Processors Forum » About the 10Mp stream of ipnc8127 rdk
Share
DaVinci™ Video Processors
  • Forums
  • Announcements
Options
  • Subscribe via RSS

Forums

About the 10Mp stream of ipnc8127 rdk

This question is not answered
Tony Li
Posted by Tony Li
on Jul 12 2012 16:16 PM
Prodigy20 points

The support for varies of resolution set (upto 10Mp)are documented in v3.0 datasheet, yet I failed to find any  selections larger than 1080p in any stream combinations. I've tried both the full and low power using NAND and SD,is there something wrong with the web GUI app?

Meanwhile,the bootloader's env seems not  changeable on  SD card, regardless of  lock state. Is there any further information about making the boot.scr? 

8127
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Jelena Kocić
    Posted by Jelena Kocić
    on Jul 30 2012 10:20 AM
    Prodigy90 points

    We have the same problem. There is no option for 10mp streaming, and release notes for GA_3.0.0 said there should be. Can someone from TI tell us something more about this. When can we expect to get 10mp streaming?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Marko Shink
    Posted by Marko Shink
    on Jul 30 2012 15:58 PM
    Genius3695 points

    Hi,

    In low-power mode,
    in GUI select :  Tri-stream ->H264+H264+MJPEG -> 10MP...

    Regards.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jelena Kocić
    Posted by Jelena Kocić
    on Aug 02 2012 05:28 AM
    Prodigy90 points

    GA_3.0.0 low power mode:

    Single and Dual steam work properly.

    Tri-stream only works with 1080p. For higher resolution (5MP, 8MP and 10MP) the displayed image is black. When you are in some of those modes and want to switch to another mode (single or dual stream which works properly at the first time), there is the message "login faled". Only camera reset solves this problem.

    In any case, there is no video stream resolutions higher than 1080p. When you choose this higher resolution in the three-stream mode, there is not shown any pictures, ie. the image is black.

    Does anyone have the same problem?

    Regards,
    Jelena

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Marko Shink
    Posted by Marko Shink
    on Aug 03 2012 10:44 AM
    Genius3695 points

    Hi Jelena,

    Can you delete old configuration files on camera. In console type :     rm  /mnt/nand/*
    Then restart camera.

    Regards.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jelena Kocić
    Posted by Jelena Kocić
    on Aug 08 2012 09:24 AM
    Prodigy90 points

    Marko,

    I tried that (deleting configuration files), but no help.
    Actually, in the meanwhile firmware was broken several times. I managed to solve that by flashing system from the beginning.

    But, at the end the camera stopped to work completly, and I got message like this:

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.
    Trying to install type control for IRQ375
    Trying to set irq flags for IRQ375
    omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
    _omap_mux_init_gpio: Could not set gpio79
    _omap_mux_init_gpio: Could not set gpio80
    omap_voltage_late_init: Voltage driver support not added
    UBI error: ubi_io_read: error -74 (ECC error) while reading 131072 bytes from PEB 1479:0, read 131072 bytes
    UBI error: torture_peb: read problems on freshly erased PEB 1479, must be bad
    UBI error: erase_worker: failed to erase PEB 1479, error -5
    UBI error: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 327:4096, read 126976 bytes
    UBI error: ubi_io_read: error -74 (ECC error) while reading 131072 bytes from PEB 1478:0, read 131072 bytes
    UBI error: torture_peb: read problems on freshly erased PEB 1478, must be bad
    UBI error: erase_worker: failed to erase PEB 1478, error -5
    UBI error: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 295:4096, read 126976 bytes
    UBIFS error (pid 1): replay_log_leb: log error detected while replaying the log at LEB 3:0
    Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
    Backtrace:
    [<c0046ba0>] (dump_backtrace+0x0/0x110) from [<c0356468>] (dump_stack+0x18/0x1c)
    r7:c4414000 r6:c006c550 r5:c002c754 r4:c04abbd0
    [<c0356450>] (dump_stack+0x0/0x1c) from [<c03564cc>] (panic+0x60/0x17c)
    [<c035646c>] (panic+0x0/0x17c) from [<c00092b4>] (mount_block_root+0x1e0/0x220)
    r3:00000000 r2:00000020 r1:c4425f78 r0:c0400e3c
    [<c00090d4>] (mount_block_root+0x0/0x220) from [<c0009454>] (prepare_namespace+0x94/0x1d4)
    [<c00093c0>] (prepare_namespace+0x0/0x1d4) from [<c00087c4>] (kernel_init+0x114/0x154)
    r5:c00086b0 r4:c04ab400
    [<c00086b0>] (kernel_init+0x0/0x154) from [<c006c550>] (do_exit+0x0/0x5e4)
    r5:c00086b0 r4:00000000

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Marko Shink
    Posted by Marko Shink
    on Aug 08 2012 16:36 PM
    Genius3695 points

    Jelena,

    UBI errors has something to do with ECC errors when using UBIFS filesystem.
    Nand blocks get marked false bad over time, so you will have to fix this with "nand scrub".
    I hope TI, or someone will fix this issue in the next IPNC release, since almost everyone has this problem.

    Before reflashing, you need to do "nand scrub" from uboot, to fix incorrectly marked nand bad blocks.
    You can check bad blocks with "nand bad".
    If you don't want to reflash uboot, then do "nand scrub" only on that nand range where kernel and filesysem are flashed.
    e.g  "nand scrub  0x280000 0xFD80000".
    Note that nand scrub will erase all data on the selected range. If you erase uboot, you will have to reflash it by CCS or SDCard.
    -------------------
    Anyway if you boot from NFS kernal + filesystem, you won't get UBI errors. And you can try 10MP from NFS.
    Or you can try SDCard boot. Look at:  IPNC_RDK_InstallGuide_Version3.0.0.pdf :  1.6.6 Flashing images to NAND Using SD Boot,  3.1.2 Boot from SD
    -----------------

    Regards.

     


     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Renjith Thomas
    Posted by Renjith Thomas
    on Aug 12 2012 14:42 PM
    Guru23890 points

    Jelena,

    I might be able to help you out with UBIFS issues. Could you please send me the following files to renjith.thomas@pathpartnertech.com?

    arch/arm/mach-omap2/board-ti8127evm.c or the relevant board file for your platform? 
    arch/arm/mach-omap2/board-flash.c
    arch/arm/mach-omap2/gpmc.c
    drivers/mtd/nand/nand_base.c
    drivers/mtd/nand/omap2.c

    Also send me the steps followed in creating/flashing the ubi image? Send the complete logs as well.

    -Renjith | www.pathpartnertech.com | Verify the answer if you think your query is resolved

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jelena Kocić
    Posted by Jelena Kocić
    on Aug 14 2012 09:11 AM
    Prodigy90 points

    Thank you all for the help and advices.
    At the moment we need to do some tests with high resolutions, so we went back at old and more stablie release Ver2.8 low power mode which has support for resolutions up to 8MP.

    Later we will come back to GA3.0.0. Maybe in meantime TI come up with some new and more stabile version.

    Regards,
    Jelena

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use