• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors » DM814x and AM387x Processors Forum » DM8148EVM S-Video output
Share
DaVinci™ Video Processors
  • Forums
  • Announcements
Options
  • Subscribe via RSS

Forums

DM8148EVM S-Video output

This question is answered
Ashwin Bihari
Posted by Ashwin Bihari
on Aug 07 2012 12:26 PM
Intellectual420 points

Hello,

I'm trying to get S-Video output working on the Mistral DM8148EVM. I've configured load-hd-firmware.sh script in /etc/init.d to not configure /dev/fb0 as the LCD output, so currently I have /dev/fb0 (HDMI), /dev/fb1 (LCD) and /dev/fb2 (S-Video).

I have a test application that can write various color patterns to the frame buffer and when I point the application to /dev/fb0 and /dev/fb1 the patterns are displayed on the HDMI and LCD without any problems. However, when I point the test application to /dev/fb2, I see my test pattern momentarily before it disappears. If I write the pattern to /dev/fb2 again, it reappears for a moment before disappearing.

Why are the frame buffer contents not being constantly refreshed to the S-Video output like they are to the HDMI and LCD outputs? I have set up VPSS as following:

./display0/mode - 1080p-60
./display1/mode - 1080p-60
./display2/mode - ntsc
./graphics0/nodes - 1:hdmi
./graphics1/nodes - 1:dvo2
./graphics2/nodes - 1:sd
./video0/nodes - vcompmux:hdmi
./video1/nodes - hdcompmux:dvo2
./video2/nodes - sdmux:sd

./display0/timings - 148500,1920/88/148/44,1080/4/36/5,1
./display1/timings - 148500,1920/88/148/44,1080/4/36/5,1
./display2/timings - 54000,720/12/68/64,480/5/41/5,0

What am I missing with my S-Video configuration?

Thanks

~Ashwin

dm8148 DM8148evm EZSDK 5.04.00.11 S-Video
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Ashwin Bihari
    Posted by Ashwin Bihari
    on Aug 08 2012 09:49 AM
    Verified Answer
    Verified by Ashwin Bihari
    Intellectual420 points

    I figured out the problem, turns out that FB0 is created and opened by the Kernel (not sure who) by default and that keeps this graphics pipeline enabled. The two frame buffers are created and started only when an application is using them and when the application closes the FB devices, all the related graphics pipeline stuff is disabled and thus the lack of output.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jon S.
    Posted by Jon S.
    on Aug 08 2012 10:00 AM
    Expert1120 points

    Any idea why there's a difference in behavior between FB0 and FB1 & FB2?  (Perhaps someone from TI hop in?)

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • HardikShah
    Posted by HardikShah
    on Aug 08 2012 22:33 PM
    Mastermind20155 points

    Hi,

    FB0 is the default framebuffer. Its used by many opensource applications like Qt, Xserver etc. I think in your case FB_CONSOLE may be opening driver. You can try disabling FB_CONSOLE using make menuconfig.

    Regards,

    Hardik Shah




    Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jon S.
    Posted by Jon S.
    on Aug 09 2012 08:25 AM
    Expert1120 points

    Hardik,

    Are you referring to CONFIG_FRAMEBUFFER_CONSOLE (under Device Drivers --> Graphics Support --> Console Display Driver Support)? 

    If so, I don't think that's the culprit, as it's not enabled in the ti8148_evm_defconfig that ships with the EZSDK. Furthermore, I double-checked my modifications to the provided defconfig and I did not enable that configuration item.

    Nothing in /proc/*/fd/* indicates usespace processes having it open. I still need to review the DM8148 fb driver code though -- perhaps this is simply by design?

    Thank you,

    Jon

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • HardikShah
    Posted by HardikShah
    on Aug 09 2012 22:24 PM
    Mastermind20155 points

    Hi,

    Are you running Qt or some application which uses fb node. Also can you see that fb is really disable once you echo 0 to to the sysfs entry. This is strange we have not seen this type of behavior.

    Regards,

    Hardik Shah




    Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jon S.
    Posted by Jon S.
    on Aug 10 2012 08:32 AM
    Expert1120 points

    Hardik,

    I think I may have caused you some confusion by not providing a clear statement of the issue. Let me try to restate the observation, as originally described by Ashwin. I'm mainly looking to understand at a high level why /dev/fbX nodes behave differently.

    • If you open /dev/fb0, write a test pattern, close /dev/fb0, the test pattern remains displayed on the output associated with /dev/fb0. The display data is not changed until another application opens /dev/fb0 and overwrites it.
    • If you open /dev/fb2, write a test pattern, and close /dev/fb2, the test pattern disappears immediately when /dev/fb2 is closed.

    If I remember correctly, fb1 and fb2 exhibit similar behavior. (Ashwin, could you verify that my description matches your observations as well?)

    My configuration is: fb0->HDMI, fb1->LCD, fb2->SD (NTSC). To address your advice, I have verified that no additional applications are using the /dev/fbX nodes while performing the aforementioned tests, and the sysfs entries all seem to be working as expected.

    Many thanks,

    Jon

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Ashwin Bihari
    Posted by Ashwin Bihari
    on Aug 10 2012 08:50 AM
    Intellectual420 points

    Jon,

    That is exactly what I'm seeing and in trying to determine why the patterns I wrote to fb1 and fb2 were disappearing, I found that the graphics1/enabled and graphics2/enabled are getting setting to 0 while graphics0/enabled stays at 1.

    I loaded vpss with 'debug=1' and looking the debug messages shows the following interesting things after all the initial configuration is done (creating the frame buffer memory and all that) I see a series of "VPSS_GRPX : create grpx0", "VPSS_GRPX : start grpx0", "VPSS_GRPX : stop grpx0" and "VPSS_GRPX : delete GRPX0" all while the system is just booting up. I haven't run my test application yet since I haven't even gotten to a prompt yet.

    The final thing that happens before I get to the prompt is the "VPSS_GRPX : create grpx0" and "VPSS_GRPX : start grpx0", there is no STOP or DELETE and thus fb0 is left running.

    When I run a test application against fb1 or fb2, I see the same sequence of messages, but I always see the STOP and DELETE messages which stops any further communication.

    I'm doing all of my testing with the pre-built images that ship with EZSDK 5.04.00.11 and not building the Kernel with my changes or anything.

    So at least as long as my application keeps the various fb's open, things should behave properly which is fine with me, but I (like Jon) am just curious as to why fb0 behaves differently without us having to do anything special with it. 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Brijesh Jadav
    Posted by Brijesh Jadav
    on Aug 11 2012 13:07 PM
    Genius10725 points

    Hi,

     

    fb0 is by default opened by other Linux drivers like console, so even when you call close for fb0, it is close completely, may be you can check open count to see if it is still opened, buy fb2 and fb3 are opened by any other Kerned drivers except the use application, so when you close, it will get removed from the display.

     

    Thanks,

    Brijesh Jadav

    Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • HardikShah
    Posted by HardikShah
    on Aug 12 2012 23:19 PM
    Mastermind20155 points

    Normally fb drivers can be opened by multiple applications. Most of the open source application writes the frame buffer once and it remains filled till you do something interactive to change the frame buffer content. Your application will be starting always after some open source application starts, which will be overwriting the buffer filled by previously open source application. So even if you close your application, open source application is still running and since buffer is over written by your application you are seeing your buffer. In our case we have QT running on our board on fb0. You can try disabling QT and than  you will see the fb0 behaving same as fb1 and fb2. Procedure for disabling QT should be there in EZSDK user guide.

    Regards,

    Hardik Shah

    Regards,

    Hardik Shah




    Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jon S.
    Posted by Jon S.
    on Aug 13 2012 08:45 AM
    Expert1120 points

    Hardik and Brijesh,

    Thank you for your additional advice and explanations.

    I'm not sure about Ashwin's setup, but I don't have the Matrix application being started by the init.d scripts (i.e. no QWS servers are keeping fb0 open). After walking through the fd's for each pid in /proc, I can say with pretty good certainty that after the system starts up, no userspace applications have the /dev/fbX nodes open.

    Hardik, are you not able to reproduce this after removing the Matrix startup from the load_hd_firmware.sh?

    Thanks,

    Jon

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Ashwin Bihari
    Posted by Ashwin Bihari
    on Aug 13 2012 08:57 AM
    Intellectual420 points

    Like Jon, I'm not running the Matrix or any other graphical application since I'm creating my own Kernel and Filesystem for my custom application. So I haven't gotten around to including my Qt application in there yet but wanted to test out all the video capture/display facilities of the Kernel before I went down the path of implementing what I need so that I'm not chasing down issues that are real and not ghosts..

    Either way, at least I know that there is a difference between the various fb's and can accommodate for them within my application.

    ~ Ashwin

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Brijesh Jadav
    Posted by Brijesh Jadav
    on Aug 13 2012 08:59 AM
    Genius10725 points

    Hi,

     

    Can you please put small printk in the FBDev driver and check if it is opened?

     

    Thanks,

    Brijesh Jadav

    Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use