8148 output now seems to only support rgb888 and yuv422 etc., will be set up to support the relevant register for dvo2 rgb565 or rgb666?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
8148 output now seems to only support rgb888 and yuv422 etc., will be set up to support the relevant register for dvo2 rgb565 or rgb666?
Hi,
You are right output of DVO is always RGB or YUV. Both RGB and YUV are 10 bits. But if you want 565 or 666. you can configure FBDEV driver to use RGB656 or RGB666. Output still will be RGB 10 bits but you can only connect MSBs of the RGB an it will be same as RGB565 in memory. Rest all bits will be replicated from the Last bit of the each component.
Regards,
Hardik shah
For the DVO port, we can not output rgb565 or rgb666 format. but there are some LCD panels that support dithering. So basically, the MSBs(5 or 6 bits) of each R/G/B component connected to your LCD data bus. the LCD will use dithering method to generate 24 bit data.
Hope this helps.
Regards,
yihe
Hi Ran,
I could not get the question, you want to have RGB666 as input or output?
Rgds,
Brijesh